RVfpga: Understanding RISC-V Architecture and Implementation on an FPGA

Kendryte K210 Board with components labeled

Intro to RISC-V

RISC-V is a relatively new computer technology that is being actively promoted as a competitor to many architectures that require fees.

RISC stands for “Reduced Instruction Set Computer”. Here the V stands for the Roman number 5. Hence RISC-V is the 5th Generation of a family of computer cores. It is pronounced “RisK Five”. Unlike most other ISA designs, the RISC-V ISA is provided at no cost with an open source license. RISC-V does not require a license because it is Open Source and Open Architecture which means that the design can be modified and special instructions can be created to improve performance or make life difficult for hackers. For more information view the introduction guide to RISC-V e-book linked here.

A growing list of products and suppliers such as Microchip, Seeed, Xilinx, Digilent are shown below:

  • Processor Boards
  • FPGA Boards
  • Resources
PolarFire FPGA Evaluation Board

MPFS-ICICLE-KIT-ES

DigiKey Part Number: MPFS-ICICLE-KIT-ES-ND

Description: PolarFire SoC FPGA SiFive RISC-V Icicle Kit MPFS250T-FCVG484EES PolarFire® FPGA Evaluation Board

 
GAPUINO Dev Kit

GAPUINO GAP8 RISC-V DEV KIT

DigiKey Part Number: 1597-1705-ND

GAP8 GAPuino - RISC-V MPU Embedded Evaluation Board

 
FE310 RedBoard RISC-V Evaluation Board

RED-V SIFIVE RISC-V REDBOARD

DigiKey Part Number: 1568-DEV-15594-ND

Description: FE310 RedBoard - RISC-V MPU Embedded Evaluation Board

 
SIPEED RISC-V

SIPEED MAIX BIT RISC-V AI+IOT

DigiKey Part Number: 1597-1714-ND

K210 Sipeed MAix BiT RISC-V AI+IoT - RISC-V MPU Embedded Evaluation Board

NEXYS A7 Trainer Board

NEXYS A7 ECE FPGA TRAINER BOARD

DigiKey Part Number: 1286-1081-ND

NEXYS A7 ECE FPGA Trainer Board

 
ARTY A7-100T: DEV BOARD

ARTY A7-100T: DEV BOARD ARTIX-7

DigiKey Part Number: 1286-1206-ND

Artix-7 Artix-7 FPGA Evaluation Board

 
T120 DEV BOARD

Trion® T120 BGA324 Development Kit

DigiKey Part Number: 2134-T120F324C-DK-ND

BGA324 Dev Kit T120 Trion® FPGA Evaluation Board

 
Xyloni® DEV BOARD

Xyloni® Development Kit

DigiKey Part Number: 2134-XYLONI-ND

Efinix T8F81C2 programmable device in an 81-ball FBGA package which is fabricated using Quantum™ technology

 
Artix-7 Evaluation Board

Artix-7 Evaluation Board

DigiKey Part Number: 1597-102991277-ND

Artix-7 FPGA Evaluation Board

GUIDE to RISC-V

RISC-V is a relatively new computer technology that is being actively promoted as a competitor to many established architectures. This guide has been written as a brief introduction for DigiKey customers and students who would like to gain knowledge of RISC-V software and hardware.

At the RISC-V Global Forum on September 3, 2020, Imagination Technologies will be announcing the “RVfpga: Complete Course in Understanding Computer Architecture” global teaching project for RISC-V as part of its university programme to be launched in November 2020. Some of the material from this course https://university.imgtec.com is presented here.

Efinix - RISC-V SOCs: Powering Embedded Computing

RISC-V is an open-source standard instruction set architecture (ISA) that is managed by the non-profit RISC-V Foundation. This modular ISA has a base instruction set and optional extension sets. Because RISC-V is free and open-source, it has gained popularity worldwide. Over 65 RISC-V cores, both commercial and open-source, are available today.

Efinix has created 3 RISC-V SoCs based on the VexRiscv core created by Charles Papon. The VexRiscv core, which won first place in the RISC-V SoftCPU contest in 2018, is a 32-bit CPU using the ISA RISCV32I with M and C extensions, has five pipeline stages (fetch, decode, execute, memory, and writeback), and a configurable feature set. Each SoC has a RISC-V processor, memory, a range of I/O, and interfaces for embedding user functions. You can easily create entire systems that include embedded compute and user-defined accelerators all in the same Trion® FPGA.

Gemstone SoC Feature Descriptions

Related Content

Bruk FPGA som snarvei til bygging av Edge AI-applikasjoner med høy ytelse og lavt energiforbruk Publish Date: 2021-01-12

Spesialisert IP og programvare lar utviklere uten FPGA-erfaring raskt distribuere FPGA-basert edge AI.

This session will appeal to anyone with an interest in embedded security in general and in RISC-V in particular.

The MultiZone™ demo shows how to secure the deterministic behavior of mixed-criticality systems where Linux and Real-Time come together in a single PolarFire SoC device.

Introduction to RISC-V Introduction to RISC V

A quick introduction to, and overview of the open-source RISC-V architecture.

Fundamentals of FPGAs—Part 5: Getting Started with Intel (Altera) FPGAs Publish Date: 2020-05-07

Developers can depend on FPGAs and other programmable devices from Intel (Altera) in a tremendous range of applications.