Webinar - Certified Smart Tracking with ISO 17025 Certified Sensors

Join Sensirion on Wednesday, April 19th at 10 AM CDT as they discuss how to lower costs by following ISO 17025 standards. How is that possible? Following these standards can help ensure more efficient monitoring, resulting in a plethora of benefits. Mathias Scharfe and Gary McNelly from Sensirion will be discussing how you can prevent the damage of goods during transit with data logging and efficient monitoring, and how tracking needs in all applications vary in terms of parameters and reliability requirements.

Sensirion is the first semiconductor company to become ISO 17025 accredited and they believe this will help the customer lower costs.

Can’t make it to the live version? Register anyway and we will send you the recording when it is complete.

Register here: https://event.on24.com/wcc/r/4169091/CDE1014D5C44FEF3904A2F0CA394D294?partnerref=blog

Om skribenten

Image of Ashley Awalt

Ashley Awalt er en utvikler av teknisk innhold som har vært hos DigiKey siden 2011. Hun har tatt en universitetseksamen i anvendt vitenskap (Associate of Applied Science) innen elektronikkteknologi og automatiserte systemer fra Northland Community & Technical College gjennom Digi-Keys stipendprogram. Hennes nåværende rolle er å hjelpe til med å lage unike tekniske prosjekter, dokumentere prosessen og til slutt delta i produksjonen av videomaterialet for prosjektene. På fritiden liker Ashley å – nja, vent litt, er det noe som er fritid når du har småbarn?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum