Although input resistance is important it is not the whole story. There is also some capacitance in these passive probes too, so they create an RC network which can load the circuit, depending on the frequencies being dealt with.
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
Although input resistance is important it is not the whole story. There is also some capacitance in these passive probes too, so they create an RC network which can load the circuit, depending on the frequencies being dealt with.
Takk skal du ha!
Hold øye med innboksen din for nyheter og oppdateringer fra DigiKey!
Angi en e-postadresse
Godta i avmerkingsboksen