When connected the scope probe takes energy from the circuit of interest. It is an additional load on the circuit which can change the shape of the signal depending on the impedance, the capacitance and the inductance.
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
When connected the scope probe takes energy from the circuit of interest. It is an additional load on the circuit which can change the shape of the signal depending on the impedance, the capacitance and the inductance.
Takk skal du ha!
Hold øye med innboksen din for nyheter og oppdateringer fra DigiKey!
Angi en e-postadresse
Godta i avmerkingsboksen