The Role of Pulse Width Modulation in Electronics

Av Nick Grillone, Applications Engineer, Same Sky

Pulse Width Modulation (PWM) is a power-control technique that regulates the effective output of an electrical signal by rapidly switching it on and off at a fixed frequency. By adjusting the ratio of the “on” time to the total cycle period, a digital source can emulate varying analog voltage levels, thereby controlling the average energy delivered to a load.

More broadly, modulation refers to altering or encoding information onto an electrical waveform to influence the behavior of a circuit or system. In practical electronics, this means shaping a signal so it can transmit data or manage how much voltage or current reaches a device. This principle is widely applied in motor drives, dimmable lighting, audio systems, and power-conversion or battery-charging circuits.

While PWM, Amplitude Modulation (AM), and Frequency Modulation (FM) are the primary strategies for manipulating a signal’s perceived magnitude or frequency, this article will concentrate specifically on PWM.

PWM basics – duty cycle and switching frequency

As mentioned earlier, PWM shapes a waveform by adjusting the effective voltage and current delivered to a load. This is achieved by rapidly driving a switching device—typically a transistor—between its fully-on and fully-off states. By varying how long the switch remains in each state, the system encodes information through the relative duration of the high and low intervals.

Practically speaking, PWM limits the net electrical power supplied to a device by altering how long it receives its full supply voltage during each switching cycle. Increasing the “on-time” raises the average output voltage, while decreasing it lowers the effective level seen by the load. Two primary parameters characterize this behavior: the duty cycle and the switching frequency.

A duty cycle represents the proportion of a complete waveform period during which a signal is in its active, or high, state. It is typically given as a percentage (%) and indicates how much of each cycle the output remains on. For instance, if a digital waveform stays high for 3 milliseconds and low for 1 millisecond, the total period is 4 ms, resulting in a 75% duty cycle and a corresponding switching frequency of 250 Hz.

Because the duty cycle directly defines the duration of the energized portion of each pulse, modifying it allows control over the effective power delivered to a load by altering the ratio of high to low time—without changing the actual supply voltage. In many systems, voltage and frequency are fixed parameters, leaving duty cycle as the primary adjustable control variable. In applications such as PWM-driven heating elements, monitoring the duty cycle can also serve as a reliable indicator that the system is delivering the intended power level.

Switching frequency describes how many times an event repeats during a given time period. In this context, the number of on-off transitions per second made by the switching device that drives the PWM signal. This rate is measured in Hertz (Hz), indicating how quickly the power stage cycles through its full operating period.

Selecting an appropriate PWM switching frequency is critical for ensuring that the load behaves as intended. If the frequency is set excessively high for a given application, mechanical components—such as relays or certain types of actuators—may be unable to keep up with the rapid transitions and can prematurely fail. Conversely, a switching frequency that is too low may cause undesirable effects such as audible noise, vibration, or instability in the controlled device. For example, while relatively low frequencies are acceptable for driving electric motors, solid-state loads such as LEDs often require significantly higher switching rates to achieve smooth, flicker-free operation.

Advantages and disadvantages of PWM

The primary benefit of PWM is its exceptional efficiency, largely because switching devices dissipate very little power. When the switch is off, virtually no current flows, and when it is fully on, the voltage drop across the device is minimal. This results in significantly reduced conduction and switching losses compared to linear control methods. Additional advantages of PWM include:

  • Lower thermal dissipation than linear regulators, thanks to its fully-on/fully-off operation
  • Seamless integration with digital logic, since the control signal is inherently binary
  • Higher overall energy efficiency when regulating motors, lighting, or power converters
  • Precise control of effective voltage or current simply by adjusting the duty cycle
  • Simplified circuitry, often requiring fewer analog components or feedback loops
  • Broad applicability across many electronic systems, from power supplies to actuators

Although PWM is a versatile and efficient technique, it does present several engineering challenges. Some of the key drawbacks include:

  • Increased switching losses at very high operating frequencies
  • Potential for voltage overshoot or transients
  • Generation of electromagnetic interference (EMI) and harmonics that may require filtering
  • Greater design complexity in high-power systems, where switching elements and layout considerations become more demanding

Switching frequencies and duty cycles in practice

Because PWM behavior is defined by both duty cycle and switching frequency, each parameter must be selected to suit the electrical and mechanical characteristics of the target load. The following product application examples—all supported by Same Sky—illustrate how these values typically vary across device types. Here are recommendations for the following electronic components:

  • Fans: Most cooling fans operate best with PWM frequencies in the 20 kHz to 25 kHz range, paired with a 0% to 100% duty-cycle window to regulate speed from fully off to maximum airflow. Higher switching rates help eliminate audible whine and produce smoother rotation. Manufacturers generally specify preferred PWM parameters to ensure proper startup behavior, speed stability, and acoustics. Same Sky supplies a wide selection of AC and DC fan hardware.
  • Buzzers: For piezo or magnetic buzzers, PWM frequencies typically fall between 1 kHz and 10 kHz, aligning with the human audible spectrum (20 Hz to 20 kHz). Varying the duty cycle adjusts sound intensity, but a 50% duty cycle usually yields a strong output with minimal distortion. Since many buzzers are tuned to a narrow resonant frequency, consulting the datasheet is essential. Same Sky carries an extensive assortment of audio buzzers.

Image of buzzer driven at ~15% duty cycle will generate a noticeably quieter tone than one operated at 50%Figure 1: A buzzer driven at ~15% duty cycle will generate a noticeably quieter tone than one operated at 50%, even at the same frequency. (Image source: Same Sky)

  • Ultrasonic sensors: Ultrasonic transducers generally rely on PWM frequencies in the 20 kHz to 400 kHz range, with a 50% duty cycle commonly used to create a clean, symmetrical ultrasonic burst. Exact values depend heavily on the specific sensor design, so manufacturer guidelines should always be followed. Same Sky offers a complete portfolio of ultrasonic sensing components.

     

  • Peltier devices: When controlling thermoelectric modules with PWM, switching frequencies between 300 Hz and 3 kHz are typically recommended. Duty cycle adjustments determine the cooling or heating output, making precise thermal regulation possible. Again, datasheet recommendations are vital for achieving long-term module reliability. Same Sky provides a wide range of Peltier devices, including single-stage, multi-stage, and integrated cooling assemblies.

Summary

Modulation refers to altering or governing the behavior of a device or system through controlled signal shaping. PWM, specifically, is a highly efficient technique for regulating power delivery in numerous electronic applications. By varying the duty cycle of a digital waveform, PWM provides precise, analog-style control while maintaining low power dissipation, making it a preferred approach for everything from motor drives to lighting, sensing, and thermal management systems.

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

Om skribenten

Image of Nick Grillone

Nick Grillone, Applications Engineer, Same Sky

Nick Grillone brings over 10 years of customer support experience to the Same Sky's Applications Engineering team. His technical and application expertise is particularly focused on our diverse range of audio components, such as microphones and speakers, as well as our sensor technology offering. In his spare time, Nick enjoys all things outdoors with his partner and his dog, including backpacking, camping, cycling, and paddleboarding.