Webinar - Which Wide Bandgap Technology is Best Suited for Your High Efficiency Application?

Wide bandgap (WBG) semiconductors are vital in today's trending technologies, including electric vehicles, green energy, and more. At this point, you’ve likely heard about Gallium Nitride (GaN) and Silicon Carbide (SiC) transistors, but what advantages do they have over traditional silicon-based power transistors? What are the differences between GaN and SiC? These are just a few questions that will be answered during the webinar with John Keller and Steven Stein from STMicroelectronics.

The webinar will be held on June 7th, 2023, at 11 AM CDT, but don’t worry if you can't attend. Register anyways and receive a recording of the webinar after it is complete.

Register here: https://event.on24.com/wcc/r/4222127/7BF6B23EE5A4414174E2C0F1846A2F4F?partnerref=blog

Om skribenten

Image of Ashley Awalt

Ashley Awalt er en utvikler av teknisk innhold som har vært hos DigiKey siden 2011. Hun har tatt en universitetseksamen i anvendt vitenskap (Associate of Applied Science) innen elektronikkteknologi og automatiserte systemer fra Northland Community & Technical College gjennom Digi-Keys stipendprogram. Hennes nåværende rolle er å hjelpe til med å lage unike tekniske prosjekter, dokumentere prosessen og til slutt delta i produksjonen av videomaterialet for prosjektene. På fritiden liker Ashley å – nja, vent litt, er det noe som er fritid når du har småbarn?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum