Graphene at DigiKey
Kennedy Labs is an excellent source for graphene, other 2D materials, and more
DigiKey is partnering with Kennedy Labs to offer graphene and other two dimensional (2D) materials to academic, industrial, and research customers looking to harness these disruptive technologies and deliver new functionality, miniaturization, gain efficiency, and lower cost in new product designs and systems.
Kennedy Labs is a manufacturer of 2D materials, heterostructures, and products enhanced by them, such as conductive inks, pastes, epoxies, and lubricants. Through their partnership, Kennedy Labs and DigiKey bring mono, bi, and tri layer CVD graphene films on copper, silicon, quartz, flexible plastic, and suspended on grids, along with various kinds and grades of graphene powders such as graphene oxide (GO), reduced graphene oxide (rGO), and graphene nanoplatelets (GnPs) to the market. Gallium oxide on sapphire and graphene on hexagonal boron nitride (hBN) on silicon substrates are available now and new 2D materials are being added as they become available.
2-D Basics: Materials for Designing the Future
In their simplest form, 2D materials are single atom layers of a particular material. Graphene, a single atomic layer of graphite, was the first such 2D to be discovered, but many other 2D materials have been discovered since then. Because of their atomic sizes, 2D materials possess amazing properties that their bulk forms do not, and they will help to usher in a new age of cutting-edge performance and miniaturization benefits to microelectronics. For example, graphene is the thinnest and lightest material known with incredible strength coming in around 300 times stronger than steel. It is also the best man-made thermal conductor and has a conductive density 1,000,000 times greater than copper.
Kennedy Labs' partnership with DigiKey has allowed them to bring the highest quality graphene development products in a range of sizes, substrates, and forms to the market. With readymade graphene on different substrates such as copper, quartz, poly, and silicon, designers can jump right in to the world of 2D material development. Kennedy Labs also offers graphene in other forms and compounds as well. For example, graphene infused ink, thermal grease, powder, thermal spreading substrates, and pastes for user enjoyment and thermal experimentation. Stay tuned for more to come from Kennedy Labs.
Kennedy Labs' Graphene and 2D Design Challenge
In order to stimulate design discussion and collaboration, Kennedy Labs invites anyone to participate in their Graphene and 2D Design Challenge. Applicants are immediately eligible for product discounts, direct factory support and/or custom development.
To enter the Kennedy Labs' Graphene and 2D Design Challenge:
- Download and complete the form
- Email form as attachment to 2DMaterials@digikey.com
- DigiKey and Kennedy Labs will review each submission carefully
Graphene
| Bilde | Manufacturer Part Number | Beskrivelse | Tilgjengelig antall | Pris | Vis detaljer | |
|---|---|---|---|---|---|---|
![]() | ![]() | KL2G-1010-SIO2/SI | 2 LAYER GRAPHENE 10MM2 SIO2 SUB | 4 - Immediate | $1,393.94 | Vis detaljer |
![]() | ![]() | KLG-RGO-1G | REDUCED GRAPHENE OXIDE POWDER | 0 - Immediate | $2,329.47 | Vis detaljer |
![]() | ![]() | KLG-1010-18CU | MONO LYR CVD GRAPHENE X4 ON CU | 0 - Immediate | $645.52 | Vis detaljer |
![]() | ![]() | KLG-1010-18CU+PMMA | CVD GRAPHENE X4 ON CU PMMA | 0 - Immediate | $711.00 | Vis detaljer |
![]() | ![]() | KLG-100100-18CU | MONO CVD GRAPHENE ON CU 4" X1PCS | 0 - Immediate | $3,732.76 | Vis detaljer |
![]() | ![]() | KLG-100100-18CU+PMMA | CVD GRAPHENE ON CU 4" PMMA X1 | 3 - Immediate | $3,901.16 | Vis detaljer |
![]() | KLG-1010-SIO2/SI | CVD GRAPHENE ON SIO2/SI X 4PCS | 6 - Immediate | $2,048.81 | Vis detaljer | |
![]() | ![]() | KLG-1010-18Q | CVD GRAPHENE ON QUARTZ X 4PCS | 0 - Immediate | $2,329.47 | Vis detaljer |
![]() | KLG-1010-175PET | CVD GRAPHENE ON PET SUB X 4PCS | 4 - Immediate | $2,011.39 | Vis detaljer | |
![]() | ![]() | KLG-1010-POLY | CVD GRAPHENE ON POLY SUB X1 PCS | 3 - Immediate | $1,157.72 | Vis detaljer |
![]() | ![]() | KL3G-1010-SIO2/SI | 3 LAYER CVD GRAPHENE SIO2/SI SUB | 6 - Immediate | $2,329.47 | Vis detaljer |
![]() | ![]() | KLG-2UM-3MMTEMAUGRID | SUSPENDED MONOLAYER GRAPHENE | 10 - Immediate | $2,797.23 | Vis detaljer |
![]() | KLG-SKIT | GRAPHENE DISCOVERY KIT 10X10 MM | 14 - Immediate | $4,668.29 | Vis detaljer | |
![]() | KLG-AKIT | GRAPHENE DISCOVERY KIT 1 WAFER | 6 - Immediate | $6,420.07 | Vis detaljer | |
![]() | ![]() | KLG-RGO-200MG | REDUCED GRAPHENE OXIDE 200MG | 8 - Immediate | $926.17 | Vis detaljer |
![]() | KLG-RGO-C-500MG | REDUCED GRAPHENE OXIDE 500MG | 2 - Immediate | $1,393.94 | Vis detaljer | |
![]() | ![]() | KLG-GOFD-1 | DRY GRAPHENE OXIDE PASTE 200MG | 0 - Immediate | $1,461.77 | Vis detaljer |
![]() | ![]() | KLG-GOPO-8 | GRAPHENE OXIDE POWDER, 1000 MG J | 0 - Immediate | $1,052.47 | Vis detaljer |
![]() | ![]() | KLG-GOPA-2 | GRAPHENE OXIDE PASTE - 50% GO, 5 | 1 - Immediate | $2,338.83 | Vis detaljer |
![]() | ![]() | KLG-GOPA-4 | GRAPHENE OXIDE PASTE, 10% GO, 5 | 5 - Immediate | $2,338.83 | Vis detaljer |