Tap to Open: How PZT Piezoelectric Ceramics Enable Smart Access Systems

The automotive industry is heading towards the era of doing away with physical switches. Front trunk and concealed door handle systems are being converted to a simple tap instead of a handle. This shift amounts to more than just aesthetic taste. You can think about this situation, opening a car door when you are not only holding groceries but also have your hands full and your fingers hard from the weather this winter.

Non-contact or semi-contact interaction is served by knock sensors. This technology is a solution that blends a modern look with great utility. The systems are more durable than mechanical switches, which wear out from repetitious use. Additionally, they are less expensive than complicated electronic touch panels. Most importantly, they are a source of intuitive user experience that is not learned but taken for granted.

The technology works on the basis of picking up on intentional taps without picking up background noise. A good system is required that can differentiate between an intentional knock and what are countless vibrations affecting a vehicle in normal operation. This is where sensing with advanced technology is critical.

Figure 1: A simple touch can unlock a car door, among other things, making design easier and more aesthetically pleasing. (Image source: BeStar Technologies)

What Does A Knock Sensor Do?

Vibration Wave Detection

When a finger strikes a metal or carbon fiber panel, it produces a mechanical wave. This wave travels through the material with speeds that depend on the properties of a material. The wave itself is not visible, but it conveys energy which can be detected. The task of the sensor is to receive this very weak mechanical signal. The wave that results from a finger tap is quite different from other vibrations. Its frequency content, amplitude and duration form a signature that is unique. A sensor located behind the panel picks up such waves by direct mechanical coupling. The panel itself serves as a transmission medium where the tap signal is transmitted to the sensor location.

Different materials transmit different kinds of vibrations with different characteristics. Metal panels are good conductors of mechanical waves. Composite materials such as carbon fiber have different acoustic properties. The sensor system must account for these variations to be reliable in any shape and with any material in the vehicles.

Signal Characteristic Identification

A vehicle is subject to constant vibrations from many sources. Such as raindrops falling against the paneling outside; automatic gas carwash blasts water at a high pressure; road surfaces that cause shocks to be transmitted via the suspension system; and wind that buffets the body panels. Each of those produces similar mechanical waves that can be same as a deliberate tap.

PZT Piezoelectric Ceramics: The Nerve Endings of Sensing Solutions

Lead zirconate titanate (PZT) is the material that makes knock sensors practical. PZT is a class of materials that have piezoelectric properties. When mechanical stress distorts the crystal formation of the material, it creates an electrical voltage. On the other hand, when we apply a voltage, it will lead to mechanical deformation.

Such conversion is instantaneous. There is no time lag between the mechanical input and electrical output. The efficiency is remarkably huge. Even tiny mechanical pressures that are measured in millinewtons cause measurable voltages. This sensitivity makes PZT ideal to detect the tap of a finger through a number of layers of auto materials.

The material's properties can be carefully modulated using by controlling the chemical composition. Different ratios of lead, zirconium and titanium lead to ceramics with different piezoelectric coefficients, temperature stability and mechanical characteristics.

Four main Benefits of PZT Piezoelectric Ceramics in Smart Interaction Systems

  1. Ultra-High Sensitivity - PZT piezoelectric ceramics sensors are used to detect knocks through heavy auto panels and interior panels. A typical vehicle door has the following components: outer skin, structural reinforcement, sound deadening material and interior trim. This makes a sandwich of quite a few centimeters in thickness. Mechanical vibrations die out as they traverse these layers, but PZT sensors receive enough signal to capture and make reliable measurements. This sensitivity arises because of the basic properties of the material.
  1. Zero Power Standby by Passive Sensing - PZT Piezoelectric Ceramics is a passive type sensor device. It produces electrical signals as power is supplied to it when mechanical input is applied and does not require any external power. This property can be used to alter the power budget for vehicle access systems. Traditional electronic sensors waste current all the time that they are monitoring for input. PZT Sensors have nothing to power them up until the moment of tap.
  2. For electric vehicles, this is so important. Every milliamp of standby current delays that time one can let a vehicle sit unused before the battery runs out of charge. PZT-based systems consume almost no current in standby, so the time taken between charges becomes longer. The sensor only needs power for the signal processing electronics which analyze the PZT output and these circuits can be in extremely low power sleep modes.

  1. Miniaturization and Invisibility Installation - PZT ceramic elements are available in an extremely thin form, often less than one millimeter. This makes it possible to install behind panels without having to make visible bulges/must cutouts. The sensor can be invisible and maintains the outside design of the vehicle.
  2. The small size also offers flexibility of installation. Engineers can place sensors in a perfect location for mechanical coupling without limiting industrial design decisions. Multiple sensors can be distributed over a panel to make larger active areas, or to be able to make location-specific commands.

  1. Wide Temperature Range and Temperature Stability - Vehicles are used in extreme conditions. Winter temperatures be reach minus 104°F in extreme environments while the summer sun can heat up dark-colored panels above 176°F. There are automotive grade PZT formulations that are consistent in their performance over this entire range. The piezoelectric effect exists at extreme temperatures, but the magnitude of the effect will change. Temperature compensation algorithms in the signal processing electronics cover any variations that may be left over to ensure that the sensitivity remains constant regardless of what the weather conditions may throw.

Core Application Scenario Analysis

  1. Automotive Front Trunk (Frunk) - Electric vehicles often locate storage compartments in the front where traditional vehicles house engines. Opening this front trunk presents a practical challenge. Users frequently approach with arms full of shopping bags, packages or other items. Reaching for a button or key fob is inconvenient. A tap-to-open system solves this elegantly. The user knocks the front panel with a knee or foot. The sensor detects this tap through the composite or metal hood. The control system verifies the proximity of the authorized key fob, then activates the electronic latch to open the compartment. The entire interaction takes under a second and requires no hands.
  2. Hidden Side Doors - Flush door handles improve aerodynamic efficiency and create clean visual lines. When the vehicle is locked, the handle retracts completely into the door panel. This presents an interface challenge: how does the user request entry?

    Traditional solutions use capacitive touch sensors that detect hand proximity. These work well but require careful tuning to avoid false triggers from rain or car washes. PZT knock sensors offer an alternative approach. The user taps on a designated area of the door panel. The sensor recognizes this pattern and commands the handle to extend.

    This approach combines well with keyless entry systems.

  3. Smart Furniture and Safes - The technology extends beyond automotive applications. Minimalist furniture designs benefit from invisible interfaces. A cabinet door with no visible handle maintains clean lines. A tap opens the magnetic latch, allowing access to contents. This works particularly well for high-end residential installations where aesthetics are paramount.
  4. Security applications also benefit. A safe with no external keyhole presents no obvious attack point. The owner taps a specific rhythm known only to them. The PZT sensors detect this pattern and release the electronic lock. This approach can supplement or replace traditional combination locks.

Conclusion

PZT knock sensors balance design aesthetics with operational convenience. They eliminate mechanical wear points that plague traditional switches. They provide intuitive interfaces that users understand without instruction. They enable invisible integration that preserves industrial design intent.

The technology has matured to the point where reliability equals or exceeds conventional solutions. Cost has decreased to make it viable for mainstream vehicle platforms, not just luxury models. As automotive manufacturers seek differentiation in competitive markets, smart entry systems provide tangible value that customers appreciate.

High-performance PZT sensing solutions are key to enhancing product value. The technology enables features that were impossible with previous approaches. It supports the transition toward more intuitive, more elegant human-machine interfaces. As vehicles become more sophisticated and user expectations rise, PZT-based sensing will play an increasingly central role in creating memorable user experiences.

Click the following link to obtain more technical and product details from BeStar Technologies, Inc.: https://www.digikey.com/en/products/result?s=N4IgTCBcDaIEIFMDKAXAhgJwAQBUEGMALAOwHsAbUgcwEsEBnQGH%2BsBJY-AOhAF0BfIA

Om skribenten

More posts by BeStar Technologies, Inc
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum