Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
LT3085-Slide2

The first three terminal adjustable regulator was introduced in 1976. It used two external resistors and generated an output voltage between 1.2V up to a maximum of 40V. It had good line and load regulation, a 3V dropout, a 1.5A output current, and a well-controlled current limit that was constant with temperature. This device was a big advance over earlier regulators which had fixed outputs and poor current limits.

PTM Published on: 2011-05-09