LT1490A/LT1491A
L7 LJUW
LT1490A/LT1491A
11
14901afd
APPLICATIONS INFORMATION
Supply Voltage
The positive supply pin of the LT1490A/LT1491A should
be bypassed with a small capacitor (about 0.01µF) within
an inch of the pin. When driving heavy loads an additional
4.7µF electrolytic capacitor should be used. When using
split supplies, the same is true for the negative supply pin.
The LT1490A/LT1491A are protected against reverse battery
voltages up to 18V. In the event a reverse battery condition
occurs, the supply current is less than 1nA.
The LT1490A/LT1491A can be shut down by removing V+.
In this condition the input bias current is typically less than
0.5nA, even if the inputs are 44V above the negative supply.
When operating the LT1490A/LT1491A on total supplies of
20V or more, the supply must not rise to its final voltage
in less than 1µs. This is especially true if low ESR bypass
capacitors are used. A series RLC circuit is formed from
the supply lead inductance and the bypass capacitor. A
resistance of 7.5 in the supply or in the bypass capacitor
will dampen the tuned circuit enough to limit the rise time.
Inputs
The LT1490A/LT1491A have two input stages, NPN and PNP
(see the Simplified Schematic), resulting in three distinct
operating regions as shown in the Input Bias Current vs
Common Mode typical performance curve.
For input voltages about 0.8V or more below V+, the PNP
input stage is active and the input bias current is typically
–1nA. When the input voltage is about 0.5V or less from
V+, the NPN input stage is operating and the input bias
current is typically 25nA. Increases in temperature will
cause the voltage at which operation switches from the
PNP stage to the NPN stage to move towards V+. The
input offset voltage of the NPN stage is untrimmed and
is typically 600µV.
A Schottky diode in the collector of each NPN transistor of
the NPN input stage allows the LT1490A/LT1491A to operate
with either or both of their inputs above V+. At about 0.3V
above V+ the NPN input transistor is fully saturated and the
input bias current is typically 3µA at room temperature.
The input offset voltage is typically 700µV when operating
above V+. The LT1490A/LT1491A will operate with their
inputs 44V above V– regardless of V+.
The inputs are protected against excursions as much as
15V below V– by an internal 1k resistor in series with
each input and a diode from the input to the negative
supply. There is no output phase reversal for inputs up to
15V below V–. There are no clamping diodes between the
inputs and the maximum differential input voltage is 44V.
Output
The output voltage swing of the LT1490A/LT1491A is
affected by input overdrive as shown in the typical per-
formance curves.
The output of the LT1490A/LT1491A can be pulled up to
18V beyond V+ with less than 1nA of leakage current,
provided that V+ is less than 0.5V.
The normally reverse-biased substrate diode from the
output to V– will cause unlimited currents to flow when
the output is forced below V–. If the current is transient
and limited to 100mA, no damage will occur.
The LT1490A/LT1491A are internally compensated to drive
at least 200pF of capacitance under any output loading
conditions. A 0.22µF capacitor in series with a 150 resis-
tor between the output and ground will compensate these
amplifiers for larger capacitive loads, up to 10,000pF, at
all output currents.
Distortion
There are two main contributors of distortion in op amps:
output crossover distortion as the output transitions
from sourcing to sinking current and distortion caused
by nonlinear common mode rejection. Of course, if the
op amp is operating inverting there is no common mode
induced distortion. When the LT1490A/LT1491A switch
between input stages there is significant nonlinearity in
the CMRR. Lower load resistance increases the output
crossover distortion, but has no effect on the input stage
transition distortion. For lowest distortion the LT1490A/
LT1491A should be operated single supply, with the out-
put always sourcing current and with the input voltage
swing between ground and (V+ – 0.8V). See the Typical
Performance Characteristics curves.