ADAM MQTT Manual
Edition V1.0 , Oct. 2017
1. Introduction of MQTT(Message Queue Telemetry Transport)
MQTT protocol is the lightweight messaging transport. Clients connect to the broker and the
MQTT message is forwarded by broker. Furthermore, ADAM is designed with features that make it
more flexible in the IoT applications.
Feature 1: Actively Publish MQTT Message
Advantech ADAM can be set up to actively publish I/O data in the form of MQTT message at a
user’s defined interval. This feature provides an efficient way to transmit data and lower the system
loading.
Feature 2: Shorten Downtime with Actively Alarm Event Notification
The alarm event is usually referred to the digital input status changes or analog input in out of the
user’s defined range. Advantech ADAM is designed with alarm trigger mechanism with instant notice.
The MQTT message will be published to broker at the moment that alarm conditions is reached.
2. MQTT Format for ADAM module
Digital Input/output module :
ADAM-6050/6051/6052/6060/6066
Description
MQTT Topic
JSON data
Firmware
Get the I/O data
of ADAM digital
input/output
module
Advantech/MAC ID /data
Example:
Advantech/0013430C981C/data
{"s":1,"t":0,"q":192,"c":1, "dix":DI
status,"dox":DO status}
D version
: V6.01B11
and higher
version
Set the value of a
digital output of
ADAM module
Advantech/MAC ID/ctl/dox
Example:
Advantech/0013430C981F/ctl/do1
{"v":DO status},
D version
: V6.01B11
and higher
version
Will Topic
Advantech/MACID/Device_Status
Example:
Advantech/0013430C981F/
Device_Status
{ "status":"Device Status",
"name":"Device
Name","macid":"MACID",
"ipaddr":"IP Address"}
D version
:V6.01B13
And higher
version

ADAM-6250/6251/6256/6260/6266
Description
MQTT Topic
JSON data
Firmware
Get the I/O data
of ADAM digital
input/output
module
Advantech/MAC ID /data
Example:
Advantech/0013430C981C/data
{"s":1,"t":0,"q":192,"c":1, "dix":DI
status,"dox":DO status}
AE version
: A1.06B02
and higher
version
Set the value of a
digital output of
ADAM module
Advantech/MAC ID/ctl/dox
Example:
Advantech/0013430C981F/ctl/do1
{"v":DO status},
AE version
: A1.06B02
and higher
version
Will Topic
Advantech/MACID/Device_Status
Example:
Advantech/0013430C981F/
Device_Status
{ "status":"Device Status",
"name":"Device
Name","macid":"MACID",
"ipaddr":"IP Address"}
AE version
: A1.06B03
And higher
version
Analog Input modules: ADAM-6017
Description
MQTT Topic
JSON data
Firmware
Get the I/O data
of ADAM
Analog input
module
Advantech/MAC ID /data
Example:
Advantech/0013430C981C/data
{"s":1,"t":0,"q":192,"c":1, "aix":AI
value,"ai_stx":condition, "dox":DO
status, "do_stx":condition}
CE version
:V5.03 B03
and higher
version
Get an analog
input range
configuration.
Advantech/MAC ID/cfg/sensor/aix
Example:
Advantech/0013430C981F/cfg/sensor/ai1
{"typ":"Range"}
CE version
:V5.04 B00
and higher
version
Set the value of a
digital output of
ADAM module
Advantech/MAC ID/ctl/dox
Example:
Advantech/0013430C981F/ctl/do1
{"v":DO status},
CE version
:V5.03 B03
and higher
version
Set an analog
input
configuration
Advantech/MAC ID/set/sensor/aix
Example:
Advantech/00D0C9F94344/set/sensor/ai1
{"typ":"Range"}
CE version
:V5.04 B00
and higher
version
Will Topic
Advantech/MACID/Device_Status
Example:
Advantech/0013430C981F/
Device_Status
{ "status":"Device Status",
"name":"Device
Name","macid":"MACID",
"ipaddr":"IP Address"}
CE version
:V5.04 B00
and higher
version

General
s: Reserved for further use, default value 1
t: Reserved for further use, default value 0
q: Reserved for further use, default value 192
c: Reserved for further use, default value 1
DI/O Module
dix: Digital Input status of channel(x-1)
example: {"di2":true} means status of DI channel 1 is true
dox: Digital Output status of channel(x-1)
example: {"do2":true} means status of DO channel 1 is true
DO status true:on, false:off
DI status true:on, false:off
AI Module
aix: Analog Input value of channel (x-1)
Note: If AI channel is disabled, AI value shows “9999.9999”
ai_stx: Condition of analog Input channel (x-1)
ai_stx value
Condition
0
Channel disable
1
Streaming, normal
2
High latch
3
High momentary
4
Low latch
5
Low momentary
do_stx: Condition of digital output channel(x-1), only for ADAM-6017 Digital output
do_stx value
Condition
1
Streaming, normal
2
DO change
Host Bmker II’)
Henrtheal keeE-Alive
typ: Input range
Range Input rage value
Range value
Input range
0-20mA
0~20mA
4-20mA
4~20mA
+-20mA
±20mA
0-5V
0~5V
1-5V
1~5V
0-10V
0~10V
0-1V
0~1V
0-500mV
0~500mV
0-150mV
0~150mV
+-10V
±10V
+-5V
±5V
+-2.5V
±2.5V
+-1V
±1V
+-500mV
±500mV
1.3 MQTT Configuration
The MQTT of ADAM can be configured by ADAM.Net utility (V2.05.11 B05 and higher version)
or ASCII command.
Note :MQTT function must be disabled before configuration and enable the MQTT function after
configuration is done.
Host (Broker IP)
Users set up the broker URL or IP address . ADAM module connection to broker over standard
MQTT protocol.
Heartbeat (keep-Alive)
The broker will regularly check the connection with the ADAM at interval of heartbeat
(keep-Alive) setting. The minimum interval setting is 5 seconds.
Dead band
Ret' n Message
Will to git
5:05 Qualitv of Service
Dead band
Dead band is set to determine the minimum interval between publishing two MQTT messages. It
is set to prevent MQTT message from publishing excessively by noise.
Retain Message
When the retain function is enabled. The broker will store the last message of the topic. If a new
subscription for the topic is made, the message will be sent to the client. Client is able to get the
last message and does not need to wait until the next message is updated.
Will topic
If the client subscribes the topic for the ADAM which is disconnected, the broker will inform the
clients by sending the will message to whom subscribe the will topic
Will Topic of ADAM: Advantech/MACID/Device_Status
Will message:
{ "status":"Device Status", "name":"Device Name","macid":"MACID", "ipaddr":"IP Address"}
Will message example:
{"status":"disconnect","name":"ADAM6051","macid":"00D0C9FEFFF5","ipaddr":"10.0.0.1"}
QoS(Quality of Service)
Users can choose the QoS level of publish/subscribe. Three levels of QoS (Quality of Service)
are defined in MQTT.
Level 0: broker/client deliver the message at most once
Level 1: broker/client deliver the message at least once
Level 2: broker/client deliver the message exactly once
Publish/Subscribe Topic
The MQTT message is forwarded by broker based on the MQTT topic. Each message contains
the data value. When client publishs MQTT message to broker, the clients who subscribe the
topic will receive the MQTT message accordingly.
lnlnmahnnl mmxk] 5mm lAdmmmml HmmlPZPIEvnnll Ammcmml ModbmAddmst
MQ'H' |
Puhhsh I 3mm
Hm ,
Hambeu
Inmvul
Rm. Meme '
wm Tupi: V
mush Q9:
Publish Tops
Subscnh: QaS .
5‘.nt mm
mm: mg 1933 —_|.
F Emu
[5— :cmnfls)
soon unflivcnnfls)
l— Emu
Advantzchflflmcgmflamwnfihm
W
AdvmmWDDCQDBlBIch/gnmxlul
AdvmmWDDCQDBIBIcfg/amx/afi
AdvmhechtflflDDCQl-VfllBlcfyamx/ai}
Advantzchflflmcgmfl Elcdldoi
AdvantzchMUWCBWB lalui/samuflnl
AdvanmhlflflWCBWflEluflwmxflafl
MVMEEWUWCBWE lBlui/semuxflui}
AdvanmhIUUWCBWZBlBIufi/semfluid
AdvanmhMUWCBWB lBIsei/semurflufi
Chld l
AdvmhechlflflDDCQDZflB/dm
AdvanMMIDWCBPZ] l Elcdldnl
Apply
1.3.1Configuration by ADAM.Net utility
Click “Cloud button” in the function list to configure the MQTT setting
Users could set up the broker URL or IP address at “Host”. Three public broker sources link are
listed in the utility
- iot.eclipse.org
- test.mosquitto.org
- broker.mqttdashboard.com
1.3.2 Configuration by ASCII
Digital input/output modules:
ADAM-6050/6051/6052/6060/6066/6250/6251/6256/6260/6266
Command
Description
Remarks
%aaSETMQTTENxx
Set MQTT enable/disable
aa: always 01
xx: 01 (enable),
00 (disable)
Return: >01
Error: ?01

%aaSETMQTTADxx…x
Set IP address of the broker
aa: always 01
xx…x: IP address/domain
(0~50 character)
Return: >01
Error: ?01
%aaSETMQTTHBxxxx
Set heartbeat interval
aa: always 01
xxxx: heartbeat interval in second
(0005~FFFF)
Return: >01
Error: ?01
%aaSETMQTTPDxxxx
Set publishing deadband
aa: always 01
xxxx: publishing deadband in
millisecond (0032~03E8)
Return: >01
Error: ?01
%aaSETMQTTPRxx
Set publishing retain
enable/disable
aa: always 01
xx: 01 (enable),
00 (disable)
Return: >01
Error: ?01
%aaSETMQTTPQxx
Set publishing Qos
aa: always 01
(xx): publishing Qos (00~02)
Return: >01
Error: ?01
%aaSETMQTTSQxx
Set subscribing Qos
aa: always 01
(xx): publishing Qos (00~02)
Return: >01
Error: ?01
ujhhhj%aaGETMQTTEN
Get MQTT enable/disable
aa: always 01
Return: !01 (enable)
!00 (disable)
Error: ?01
%aaGETMQTTAD
Get IP address of the broker
aa: always 01
Return: !IP Address/Domain (IP
Address/DomainName)
Error: ?01
%aaGETMQTTHB
Get heartbeat interval
aa: always 01
Return: !xxxx (heartbeat interval in
hex format)
Error: ?01
%aaGETMQTTPD
Get publishing deadband
aa: always 01
Return: !xxxx (deadband in hex
format)
Error: ?01
%aaGETMQTTPR
Get publishing retain
enable/disable
aa: always 01
Return: !00 (enable)
!01 (disable)
Error: ?01

%aaGETMQTTPQ
Get publishing Qos
aa: always 01
Return: !xx (publishing Qos in hex
format)
Error: ?01
%aaGETMQTTSQ
Get subscribing Qos
aa: always 01
Return: !xx (subscribing Qos in hex
format)
Error: ?01
Analog input modules
ADAM-6017
Command
Description
Remarks
%aaSETMQTTENxx
Set MQTT enable/disable
aa: always 01
xx: 01 (enable),
00 (disable)
Return: >01
Error: ?01
%aaSETMQTTADxx…x
Set IP address of the broker
aa: always 01
x…x: IP address/domain
(0~50 character)
Return: >01
Error: ?01
%aaSETMQTTHBxxxx
Set heartbeat interval
aa: always 01
xxxx: heartbeat interval in second
(0005~FFFF)
Return: >01
Error: ?01
%aaSETMQTTSTxxxxxxxx
Set publishing data streaming
interval time
aa: always 01
xxxxxxxx: publishing data streaming
interval time in millisecond
(0032~FFFFFFFF)
Return: >01
Error: ?01
%aaSETMQTTPRxx
Set publishing retain
enable/disable
aa: always 01
xx: 01 (enable),
00 (disable)
Return: >01
Error: ?01
%aaSETMQTTPQxx
Set publishing Qos
aa: always 01
(xx): publishing Qos (00~02)
Return: >01
Error: ?01

%aaSETMQTTSQxx
Set subscribing Qos
aa: always 01
(xx): publishing Qos (00~02)
Return: >01
Error: ?01
%aaGETMQTTEN
Get MQTT enable/disable
aa: always 01
Return: !01 (enable)
!00 (disable)
Error: ?01
%aaGETMQTTAD
Get IP address of the broker
aa: always 01
Return: !IP Address/Domain (IP
Address/DomainName)
Error: ?01
%aaGETMQTTHB
Get heartbeat interval
aa: always 01
Return: !xxxx (heartbeat interval
in hex format)
Error: ?01
%aaGETMQTTST
Get publishing data streaming
interval time
aa: always 01
Return: !xxxxxxxx (data streaming
in hex format)
Error: ?01
%aaGETMQTTPR
Get publishing retain
enable/disable
aa: always 01
Return: !00 (disable)
!01 (enable)
Error: ?01
%aaGETMQTTPQ
Get publishing Qos
aa: always 01
Return: !xx (publishing Qos in hex
format)
Error: ?01
%aaGETMQTTSQ
Get subscribing Qos
aa: always 01
Return: !xx (subscribing Qos in
hex format)
Error: ?01
a was amp Help
Search Device
Add Davina: {a Gmup
Group Canfigmah'on
Term-l ‘ov Comm-mi mung
PrimSaeen
Hm F.4- Picky-v
Mow-inn sueeWEvem Dam
mm M m Pan
Mam GCL D on. Maw
Mow-«m APAX
wsz ,
ADAM MQTT
Mm m cum I:
WM [m 1 WW. -
M "W, mm mm. W m ”mg
m w w \m \s \
mm.“ a» mm mm"...
\uv ‘
1.4 How to start the MQTT with ADAM
ADAM.Net utility provides the pages to simulate MQTT client to test the MQTT of ADAM modules.
Users are able to experience the benefits of the ADAM with MQTT in 4 steps.
Step 1 :Click “Tools” and “MQTT”, the page will forward to ADAM MQTT page
Step 2 :Set up the connection
In the connection configuration page, user is able to set up the client information. The default host is
public broker source” iot.eclipse.org” at port 80. Users can also set up the host URL or IP address.
Click “connect” when the configuration is done.
Note: 1. Path, Username, Password, TLS, Clean session function is not released
2. The webpage only supports the connection to broker over WebSocket
Mn my: w— EDI
Ammmmmsm ('s" w nrqv‘ «92 v I.‘mlmm‘>m1mlm.m‘mxmy mm'dis‘m'flm'flmgmytu: «oa- cm W'IsgmleMflW
mmmrramm ('vvue) :mmmm 1511 m: n
mmmmmum Prune] mummies u ”2522 n
m Hyman m a.“
mmmam. (-5- w mpg-m 'L'1rm1'Iluawrzmm‘wmkmmwmuw was ummm-ummmm-mT mw-uu,-ammswu
erzmmm (Tum magnum: m1 m: n
mnmmfimm fv' m; momma “492522 0
Step 3: Subscribe/Publish function
Subscribe
Users set up the topic and choose the QoS level, then click the subscribe button. The message of the
topic will be shown in the history field.
Publish
Set up publish topic, QoS and message, then click Publish button. The MQTT message will be
published to the broker. If the retain function is enabled. ADAM will receive the last message when
subscribes the topic.
Step 4: Review the MQTT Message
Users can read the last MQTT message and the historical messages in last message column and history
column.
Last message of ADAM module
History message of ADAM module
Products related to this Datasheet
MODULE TCP 12CH DGTL I/O
MODULE TCP ISO 16CH DGTL I/O
MOD I/O TCP 15-CH DIGITAL
MODULE TCP ISO 14CH DGTL I/O
MODULE TCP 6CH DGTL I/O
MOD 4-CH RELAY OUTPUT TCP
MOD 16-CH INPUT TCP
MOD REMOTE 8-CH ANLG INPUT TCP